Transfer Controller CAFs to Computer - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
Note: See Getting Started with Trunk Utilities before completing the following steps.
  1. Create a folder on your local computer where you would like to save the CAFs.
  2. From the Tools menu, select Trunk Utilities > Transfer Controller CAFs to Computer. The Trunk Utilities - Transfer Controller CAFs to Computer wizard appears with the Connection screen active.

  3. Select the desired connection type and parameters and click Next. The Controller Transfer screen appears.

  4. Do one of the following:
    • Click Discover to begin the discovery process and locate devices. When devices are located, they appear in the main section of the Transfer screen.
      Note: To stop the Discover process, click Stop.
    • Click Browse to select a template file, if desired. The Open dialog box appears. Browse to and select the transfer template, and click Open.

  5. Select the devices from the list.

    Note: If more than one device has the same Instance Number, the numbers display red in the device list.
  6. Select or clear check boxes next to the devices you want to transfer CAFs from to the computer.

  7. Click the Browse button next to the Directory to Save Files to Computer field. The Select Directory dialog box appears.

  8. Browse to and select the desired directory in which to transfer the device CAFs from to the computer, and click Open.

  9. If you imported a device from a transfer template, select the device and click Get Device Info. The Get Device Info button only works for devices that were imported from a transfer template. This is because the transfer template does not store the device model or Boot and Main Code versions.
  10. Click Finish. The CAF transfer process to computer begins.

  11. Check the progress of the transfer to computer as follows:

    • View the text in the Status column.

    • Click View Status. The Status dialog box appears showing current status of the operation. Click Refresh periodically to update the status. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad.

    • Click View Log. The Log dialog box appears showing the detailed operation log file. Click Refresh periodically to update the log. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad.

    • Click Clear Log if needed. This action clears the contents of the log file.

  12. When the transfer to computer completes, click Done.