This Select Attribute dialog box is used by the Transfer CAF and Attributes to Controller, Read/Write Attributes Online, and Attribute Template utilities. The dialog box displays a representation of all the possible points in a tree format.
Field |
Description |
---|---|
Show All |
Use to view all points. If this option is not selected, only BACnet exposed points appear. |
Filter | Provides a field to search the selection tree based on the node name. The search results include the matching node and its ancestors. |
OK |
Saves the selections and closes the dialog box. |
Cancel |
Closes the dialog box without saving. |
|
Opens the Help system. |