About this task
The Transfer CAF and Attributes to Controller option through Trunk Utilities allows you to transfer an open CAF file to multiple devices on the same trunk and mass edit attributes using attribute templates and read/write functionality. Access this utility from the Tools menu by selecting Trunk Utilities > Transfer CAF & Attributes to Controller. This menu option is only available when a CAF is open.
With the Transfer CAF and Attributes to Controller option through Trunk Utilities, the application files are transferred in parallel, which is more efficient than the serial application file transfer in the Transfer CAFs to Multiple Controllers option.
After selecting the devices and working with the attribute template, the utility transfers code to the devices in the following order: