Working with the Trunk Utilities - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Trunk Utilities allow you to perform a transfer to a computer or device and upgrade multiple devices on the same trunk at once, as well as mass edit attributes of multiple devices on the same trunk using attribute templates.

To transfer to the computer or transfer to a single device, see the Transfer Operations section. For information on upgrading a CAF or using the Bulk CAF Upgrade Utility, see the Upgrading System Files section.