Zone (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This module is a Zone Temperature Input and it is always provided. All the Zone Temperature options assume that a model of the Network Sensor family is being used for Temperature, the Setpoint Adjust options of Common Setpoint Adjust or Warm Cool Adjust, a Temporary Occupancy interface from the Network Sensor, and Humidity input from the Network Sensor. Refer to the Network Sensors product literature to match the functionality selected for the application with a specific Network Sensor hardware model. See the ZN-T Setpoint Determination section for details on how this module works.