Lighting (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Lighting option creates an output to interface a Lighting Relay. If the lighting option is selected, the Always Occupied selection in the Occupancy (VAV-SD) section is not available. Only the Occupancy Mode Determination Mode logic interfaces with the Lighting Output. The default output configuration is a single, maintained binary output.