System OK (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This feature determines whether the VAV is in an OK state. The system is considered OK when it is proven on, it is achieving its temperature or pressure setpointss for at least 5 minutes, and it is ready and able to serve its load, it is not in a state of startup or alarm.