Optional Features (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Optional Features selections provide Network Inputs modules for supervisory system interfaces to override the main applications sequence of operation through connections to the appropriate Setpoint/Miscellaneous modules or State Generators.