The Details dialog box displays software and hardware attributes/parameters for modules or logic blocks.
Screen Area |
Description |
---|---|
Edit Button |
Enters Edit mode and allows modification of items in the view. |
Apply Button |
Saves the changes to items in the view. |
Cancel Button |
Cancels the edits made and exits Edit mode. |
Attribute Table |
Lists the selected module/block’s attributes/parameters, their defined values, and units. Note: If the Name field is blank, the Standard Name appears in the UI.
See the Modules, Logic, and Input and Output Objects sections. |
Input and Output Tables |
Displays both an Inputs and an Outputs table for the selected module/block. These tables include the following data:
Note: If there are no inputs and outputs for a module (as is commonly the case for Network Inputs), this panel appears hidden and cannot be opened regardless of the previously displayed view.
See the Modules, Logic, and Input and Output Objects sections. |
|
Opens the Enum Finder for advanced searching of enum sets. |
IO Modifications Check Box |
Enables you to add or remove inputs and outputs. |
Close Button |
Closes the Details dialog box. |
|
Opens the Help system. |