Simple View Workspace - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This workspace contains the Application and System Selection Information tabs. You can view inputs, outputs, and parameters using the Application tab, or view system configuration selections using the System Selection Information tab. See the Application Tab and System Selection Information Tab sections for information.