CCT provides two ways to change Release modes. See Changing Release Modes and Selecting a System for further information.
The current release mode of your application is shown both in the status bar and the application title bar. Unique preferences for system selection, common object naming, and default controllers are preserved when changing between Release modes.
Corresponding Firmware
- CAF upgrades are allowed if your current Release mode is newer than the Release mode that the CAF was created in, and if the CAF is in the same device family as the current Release mode.
- CAFs from older Release modes can be opened and commissioned, but some attributes may not display as expected.
- The controller tool prompts users to switch to the matching Release mode (required for editing or upgrading) or to open read-only. Editing CAFs is restricted to changing the default value property on your objects, if you do not upgrade the CAF to the current Release mode.
Simulation and Release Mode Compatibility
Release Modes and Software Tool Release Functionality
The software tool's release version is independent from the CAF's Release mode—allowing you to switch between Release modes without losing software tool functionality. All software UI features remain accessible to you for the current tool no matter what Release mode you work in. For example, if you are working in Release Mode 10.2 / Firmware 6.2 you will have the same features.
See also Changing Release Modes.