Launch Wizard - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Launch Wizard appears in the Control Block palette before the folders containing available blocks for selection. After you select a module within the Activities tree, you can drag the Wizard to the logic diagram workspace to launch the New Module Selection dialog box. Within this dialog box, you can select multiple logic blocks to add to the module. When you click Finish, the logic blocks appear in the logic diagram. Adjust the placement of the blocks as needed.

See Using the Launch Wizard in the Configuring a System section.