Features Panel - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Features panel appears across the bottom of the Classic View workspace. You can view this panel regardless of the application tab that currently appears.

Different trees and features appear depending on if the controller is an Advanced Application, General Purpose, or VAV Controller.

Depending on the mode in which the tool is operating, you are able to perform certain tasks in the Features Panel. For information on the modes, see the Modes section. The following table describes the tasks you can perform in the panel in the different modes.

Table 1. Panel Tasks Available in Different Modes

Task

Mode

Configuration

Simulation

Commissioning

View Connections

(Connections)

X

X

X

Modify Connections

(Connections)

X

   

View Parameters

(Parameters)

X

X

X

Modify Parameters 1

(Parameters)

X

X 2

X2

Configure the Display

(Display)

X

   

View the State Tables

(State Tables)

X

X

X

Modify the State Tables

(State Tables)

X

   

View Advanced Program Features

(Advanced Data)

X

 

X

Modify Advanced Program Features

(Advanced Data)

X

 

X 3

View BACnet Exposed Information

(BACnet Exposed)

X

X

X

1 You cannot modify outputs of modules from the Parameters table.
2 Select parameters only.
3 You can edit the details of advanced features in Commissioning mode, but you cannot add or delete advanced objects in this mode.