Output Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Output Control category appears in the Control tab (Figure 1). This section lists the output controllers defined for the system. An output control module defines the specific logic associated with each state, as determined by the State Tables’ mode. For example, if the State Tables determine that the Proportional Box Heating Control output controller should be in Control mode, the Proportional Box Heating Control output controller defines the PID control logic to use while in this state.

During simulation and commissioning modes, the Output Control category displays a third row of text. This row provides the status from the state generator that is in control and the name of the State Generator module that is generating the state. The status is shown in parentheses followed by the text Generated by: and the name of the State Generator module. For example, (Satisfied) Generated by: Zone Temperature Determination.

See Output Control Modules for information. .

Back to Control Tab Module Categories