This workspace contains the Control and Logic tabs. You can view an overview of a system using the Control tab, view the logic of the entire application or individual modules using the Logic tab, or view additional system details using the System information link on the status bar. See the Control Tab and Logic Tab sections for more information.