System Selection Updates - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

After you upgrade the CAF, you have the option to replace the logic originally created by System Selection to receive the updated modules and the functionality found for the system types in Table 1.

Important: All previous user modifications are lost if you make changes to the system selections. (Lost changes include: sideloops, user added inputs, outputs, network inputs, network outputs, modules, changes in state tables, parameters, logic, and input/output setup.)
Important: Rerunning the System Selection wizard on an application created at the current software release reflects the exact selections made previously. When you rerun the System Selection wizard on an application created with software at a release earlier than Release 5.1, we recommend that you check the selected nodes in the tree to ensure that they match the equipment properly before completing the System Selection wizard. This recommendation is especially important for AHU, Central Cooling, Central Cooling with Optimization, and Central Heating applications, as these applications have been updated with new and updated selection options over time.

Table 1 lists system types and their changes since the last release of the tool. Use this table to help determine whether to modify the System Selection. See Rerunning System Selection for more information.

Table 1. System Selection Tree Updates

System Selection Tree

Description

All System Types

No overall changes since the last release.

AHU Mixed Air Single Duct Applications

The System Selection Tree for all AHU and RTU standard control sequences now includes a new node, First Stage Modulated under the Cooling sub-node of Coils. Refer to Staged Cooling (MASD).

AHU 100% Outdoor Air Single Duct Applications

The System Selection Tree for all AHU and RTU standard control sequences now includes a new node, First Stage Modulated under the Cooling sub-node of Coils. Refer to Coils (Cooling) (OASD).

AHU Mixed Air Dual Duct Applications

The System Selection Tree for all AHU and RTU standard control sequences now includes a new node, First Stage Modulated under the Cooling sub-node of Coils. Refer to Coils (Cooling - Cold Deck) (MADD).

AHU 100% Outdoor Air Dual Duct Applications

The System Selection Tree for all AHU and RTU standard control sequences now includes a new node, First Stage Modulated under the Cooling sub-node of Coils. Refer to Coils (Cooling - Cold Deck) (OADD).

AHU Rooftop Unit Applications

The System Selection Tree for all AHU and RTU standard control sequences now includes a new node, First Stage Modulated under the Cooling sub-node of Coils. Refer to Coils (Cooling) (RTU).

AHU Multizone (Mixed Air Dual Duct) Applications

The System Selection Tree for all AHU and RTU standard control sequences now includes a new node, First Stage Modulated under the Cooling sub-node of Coils. Refer to Coils (Cooling - Cold Deck) (MADD-MZ).

Fan Coil Applications

No changes since the last release

Unit Ventilator Applications

No changes since the last release

Heat Pump Applications

No changes since the last release

VAV Single Duct Applications

No changes since the last release

VAV Dual Duct Applications

No changes since the last release

VAV Slave Single Duct Applications

No changes since the last release

VAV Slave Dual Duct Applications

No changes since the last release

Central Heating Applications

No changes since the last release

Central Cooling Applications

The system selection tree for Central Cooling Applications now includes the sub node CHW Pump Speed under the Chillers node. Refer to Chillers (CC). There is also a new node Waterside Economizer. Refer to Waterside Economizer (CC).

Central Cooling with Optimization Applications

No changes since the last release

Custom Applications

No changes since the last release

Monitoring Supervisory Control Only Applications

No changes since the last release

Sideloop Applications

No changes since the last release