New Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Table 1 lists and describes the new modules that have been added to the system since the last release.

Table 1. New Modules

Module

Description

Damper Command OR

Output Control: Provides OR logic for damper control.

Exhaust Damper Control

Output Control: Provides control logic for the exhaust damper position in flow control modules, based on the VAV-Supply Damper Control v51 module.

Subordinate Supply Flow Setpoint Control HFR

Output Control: Provides flow setpoint controlled by the Supply Damper Control module. This module uses a heating flow reset strategy.

Secondary Bypass Valve Sequencing

State Generation: Provides control logic for secondary bypass valve PID, based on system enable and output of the secondary pumping PID.

Application Mode Override

State Generation: Enables user to override the current AHU operation mode.

Status AND

Setpoint/Miscellaneous: Provides AND logic for the dual pump status.

N2 VAV DD Common Outputs Output Control: Translates the controllers' cooling control status commands into the outputs required for the legacy application.
N2 Terminal Mode Input Setpoint/Miscellaneous: Translates the N2 mode commands into the outputs required for the legacy application.
N2 VMA DD Mode Input Setpoint/Miscellaneous: Translates the VAV Dual Duct Box Mode, Water Flush, Warmup Command, and Cooldown Command into outputs required for the legacy application.