Position Feedback (UV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Position Feedback selections provide analog and binary inputs for modulated damper outputs. Position feedback adds an input for each output that indicates the actual position of the controlled device. Analog feedback uses a voltage or resistance signal to span 0-100% position, and binary feedback uses one or two binary inputs to indicate position (OPEN, CLOSED, or OPEN and CLOSED). These feedback inputs are for monitoring purposes only. If you want to generate an alarm or other functionality using the position feedback inputs, you must create custom coding to do so.

The selection options for Position Feedback are:

  • Modulated Damper Outputs

    • No Position Feedback

    • Analog Input per Output

    • Binary Input per Output

  • Modulated Valve Outputs

    • No Position Feedback

    • Analog Input per Output

    • Binary Input per Output

  • Two Position Valve Outputs

    • No Position Feedback

    • Binary Input per Output

    • Two Binary Inputs per Output