Monitored Safeties (UV) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Discharge Air Smoke Detector and Low Limit Temperature Switch selections create optional Sensor points that can be mapped to the Supervisory system and alarm points created.

The selection options for Monitored Safeties are:

  • Discharge Air Smoke Detector

  • Low Limit Temperature Switch