Transfer to Device (Download) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

You can transfer your open CAF to a device and update the firmware of that device or attached SA Bus devices by using the Transfer to Device (Download) command.

You can only initiate the Transfer to Device (Download) when your CAF has a fully bound (hardware-assigned) system. To upgrade the firmware of a ZFR device, see Upgrade Single ZFR Coordinator.

The Transfer to Device (Download) feature is disabled for unlicensed devices.