Staged Device Enable Determination Series - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Staged Device Enable Determination Series module ensures that airflow is enabled before VAV Staged Box Heating Control is enabled. The module interlocks with a series fan command, or checks that the supply flow is greater than the minimum heating flow setpoint (when there is a box fan) before enabling the staged heating.