Attributes (Staged Device Enable Determination Parallel) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Staged Device Enable Determination Parallel module.

Table 1. Staged Device Enable Determination Parallel Attributes

Name

Type 1

Description

Default Value

Fan Mode

 

Indicates whether the fan is currently commanded on.

Off

Set Name: Off/On

State

G

Provides the desired status to Staged Enable.

False

Set Name: False/True/Fault

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)