Reliability (Fan Determination [VAV Series]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This module always uses the last reliable value received if any of the inputs should become unreliable. The default value of the input is used if the signal to it has never been reliable.