Module Use in Applications (Fan Determination [VAV Series]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual module in this group using the name in the following table.

Table 1. Fan Determination (VAV Series) Uses in Application System Selection Trees

Module Instance Name

Applications

Series Fan Determination

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.