The following table describes the attributes used by the VAV Unocc Status Determination modules.
Name |
Description |
Default Value |
---|---|---|
Box Heating Control Status |
Used to indicate to this module that it can affect the box heating output. |
Overridden Set Name: Control Status |
Cooling Setpoint |
Desired unoccupied cooling temperature setpoint. |
28 °C, 82 °F |
Detailed State |
Contains the detailed unocc state giving devices requested. |
Set Name: VAV Unocc Detailed |
Heating Priority |
Indicates which heating to use first when both box and supplemental heating exist. |
Supplemental Set Name: VAV Heating Priority |
Heating Setpoint |
Desired unoccupied heating temperature setpoint. |
16 °C, 61 °F |
Occupancy |
Contains the current Occupancy mode as determined by Occupancy Mode Determination. |
Occupied Set Name: Occ Effective |
State |
Current state of the hybrid activity. |
Set Name: Unoccupied Status States |
Supp Heating Control Status |
Used to indicate to this module that it can affect the supplemental heating output. |
Overridden Set Name: Control Status |
UNOCC-SATTIME (Satisfied Timer Duration) |
Time that the Zone Temperature must be within the limits before switching to Satisfied. |
30 Seconds |
UNOCC-STATE (Unocc Status) |
Contains the current unoccupied status. |
Set Name: VAV Unocc Status |
WarmupCooldown |
Current WarmupCooldown State. |
Normal Set Name: OST Warmup Cooldown |
Zone Temperature |
Current Zone Temperature. |
22 °C, 72 °F |