Attributes (Unit Enable Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Unit Enable Determination modules.

Table 1. Unit Enable Determination Attributes

Name

Type 1

Description

Default Value

Hardware Mode

 

Specifies whether to allow the unit to operate normally or to shutdown.

Enable

Set Name: Shutdown/Enable

Network Mode

 

Specifies whether to allow the unit to operate normally or to shutdown.

Enable

Set Name: Shutdown/Enable

PFRESTART-EN (Power Fail Restart Enable)

 

Specifies that, when this value is set to true, a timer holds the output at shutdown until the Power Fail Restart Time elapses.

False

PFRESTART-TIME (Power Fail Restart Time)

 

Specifies that, when the power fail restart logic is enabled, the start is delayed by the time specified in this value.

60.0 Seconds

Resolution Mode

 

Used when both inputs are connected to determine how the two input commands (network and hardware) should be resolved into a single output command.

Either Can Shutdown

Set Name: Resolution Mode2

UNITEN-STATE (State)

G, V

Current desired state for the unit.

Set Name: Shutdown/Enable

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)