Primary States (Occupancy Mode Determination [MZ]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The module behaves in the same manner as the base Occupancy Mode Determination module. The eight Zone X Temp Occ inputs are assumed to be momentary(only active for a few seconds at a time and up to a minute for remote sensors). If an input remains active for long periods of time, the module may not be able to detect other zones requesting temporary occupancy.