Reliability (Energy Hold Off Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
Table 1. Energy Hold Off Determination Reliability

Input

Behavior When Input Is Not Reliable

Hardware Mode

Specifies that when the Hardware Reliability is False the State output matches the Network Mode if the Network Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Normal.

Network Mode

Specifies that when the Network Reliability is False the State output matches the Hardware Mode if the Hardware Reliability is True. If both Hardware Reliability and Network Reliability are False, the output is Normal.