Attributes (Energy Hold Off Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The following table describes the attributes used by the Energy Hold Off Determination modules.

Table 1. Energy Hold Off Determination Attributes

Name

Type 1

Description

Default Value

EHO-STATE (State)

G, V

Contains the state output generated from the Network mode and Hardware mode inputs based on the Resolution Mode setting.

Set Name: Normal/Energy

Hold Off

Hardware Mode

 

Specifies whether to allow the unit to operate normally or in Energy Hold Off.

Normal

Set Name: Normal/Energy

Hold Off

Network Mode

 

Specifies whether to allow the unit to operate normally or in Energy Hold Off.

Normal

Set Name: Normal/Energy

Hold Off

Resolution Mode

 

Used when both inputs are connected to determine how the two input commands (network and hardware) should be resolved into a single output command.

Either Can Activate

Set Name: Resolution Mode

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)