AHU applications have an Application Mode input that allows you to force the unit into a mode of operation. The possible modes are Cool Only, Heat Only, Fan Only, Water Flush, Purge, Vent, and Auto. This module separates the Water Flush mode to a separate output to allow it to be separately connected to State Selection.
You can view and modify the modules in this group’s logic.