Attributes (Occupied Zone Sequencing [HP]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Occupied Zone Sequencing (HP) module.

Table 1. Occupied Zone Sequencing (HP) Attributes

Name

Description

Default Value

Cooling Control Status

Contains the value fed back from the cooling controller necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

Cooling Setpoint

Contains the desired zone temperature when under cooling control.

23 °C, 74 °F

Damper Control Status

Value fed back from the damper controller necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

Discharge Air Temperature

Contains the value that is to be compared to the Discharge Air Low Limit (DALL) and is used to determine whether it is necessary to enter DALL control to modulate the OA Damper closed to keep the discharge air temperature from falling below the DALL.

22 °C, 72 °F

Fast Sequence Enabled

Allows the user to enable or disable the transition to satisfied when the setpoint changes by more than the Setpoint Threshold.

True

Free Cooling Available

Indicates whether economizer cooling is available.

False

Heating Control Status

Value fed back from the heating controller necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

Heating Percent Cmd

Indicates the current command from the heating controller that operates first. This signal comes directly from the PID in the output controller module.

0.0

Display Units: %

Heating Setpoint

Contains the desired zone temperature when under heating control.

21 °C, 70 °F

Low Limit Setpoint

Contains the low limit for the Discharge Air Temperature.

13 °C, 55 °F

Occupancy

Accepts the current occupancy status.

Occupied

Set Name: Occ Effective

Setpoint Threshold

Contains the value used to determine whether a significant setpoint change has occurred.

1 °C, 2 °F

Supp Heating Control Status

Contains the value fed back from the supplemental heating controller necessary for the sequencer to determine what actions to take.

Overridden

Set Name: Control Status

ZNT-STATE (State)

Represents the current state generated by the heat pump zone temperature sequence.

See Primary States (Occupied Zone Sequencing [HP]).

Satisfied

Zone Temperature

Contains the measured temperature in the zone.

22 °C, 72 °F