Primary States (Occupied Zone Sequencing [FC/AHU]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Heating: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint.

  • Satisfied: The sequencer is in this state when the Zone Temperature is greater than the Heating Setpoint and the Zone Temperature is less than the Cooling Setpoint and both the Heating and Cooling Control Status’ are Low. The sequencer may also go to Satisfied when Fast Sequence Enabled is True and the Zone Temperature is between the Heating and Cooling Setpoints and Heating Setpoint was decreased by more than the Setpoint Threshold or the Cooling Setpoint was increased by more than the Setpoint Threshold.

  • Cooling: The sequencer is in this state when the Zone Temperature is greater than the Cooling Setpoint.

  • Temperature Unreliable: The sequencer is in this state when the Zone Temperature is not reliable.