Module Use in Applications (Occupied Sequencing [Single Device]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupied Sequencing (Single Device) Uses in Application System Selection Trees

Module Instance Name

Applications

Preheat Sequencing

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications 1

AHU 100% Outdoor Air Dual Duct Applications 2

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.

1 The AHU Mixed Air Dual Duct and Multizone applications use both Preheat Sequencing and Mixed Air Hot Deck Sequencing.
2 The AHU 100% Outdoor Air Dual Duct application uses 100 OA Hot Deck Sequencing instead of Preheat Sequencing.