Occupied Sequencing (Single Device) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Occupied Sequencing (Single Device) module generates the appropriate temperature control state for a single heating or cooling device in an Air Handling Unit (AHU) application. This module can be used when the preheat device controls the mixed air temperature, the heating device controls the hot deck temperature, or the cooling device is not sequenced with preheat or economizer such as a cooling only 100% Outdoor Air Unit. This module accepts the temperature and setpoint inputs as well as the control status. For information on how the FSM determines the state, see FSM (Occupied Sequencing [Single Device]).