Module Use in Applications (Occupied Sequencing [AHU MADD w HR]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupied Sequencing (AHU MADD w HR) Uses in Application System Selection Trees

Module Instance Name

Application

Mixed Air Cold Deck HR Sequencing

AHU Mixed Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.