Occupied Sequencing (AHU MADD w HR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Occupied Sequencing (AHU MADD w HR) module generates the appropriate temperature control state for the cold deck on a mixed air dual deck AHU application. This module accepts the temperature and setpoint inputs listed in the attributes table as well as the heating, cooling, and damper control statuses. For information on how the FSM determines the state, see FSM (Occupied Sequencing [AHU MADD w HR]).