Occupied Sequencing (AHU MADD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Occupied Sequencing (AHU MADD) module generates the appropriate temperature control state for the cold deck on a mixed air dual deck Air Handler Unit (AHU) application. This module accepts the temperature and setpoint inputs as well as the heating, cooling, and damper control statuses.