Coil Circulation Pump Sequencing - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Coil Circulation Pump Sequencing provides Less Than or Equal logic. This logic block is laid down by the Coils > Coil Pump > Low Temperature Circulation selection in the Air Handling Unit Applications. If the Outdoor Air Temperature is less than the Low OA-T Setpoint, the pump is called to run. See the Less Than or Equal description in the Compare topic of the Logic section.

To see a module's connections and how modules interact with it, view the Connections table.