Attributes (Analog Override Check) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Analog Override Check module.

Table 1. Analog Override Check Attributes

Name

Type 1

Description

Default Value

Number of Input Attributes

 

Indicates the number of inputs evaluated by this module. The module calculates this value.

1

Output n Priority

 

Indicates the current priority of the monitored analog output.

0

Display Precision: 1s

Output Overridden

G

Indicates whether the output is overridden.This output value is set to True when Setup equals AND, and all of the Output n Priority inputs show that the output objects being monitored are in an Overridden State (that is, the value is greater than zero and less than 16).

This output value is set to True when Setup equals OR, and any of the Output n Priority inputs show that the output objects being monitored are in an Overridden State.

False

Setup

 

Indicates whether the value of Output Overridden is set to True when all of the Output n Priority inputs are not 0 or 16 (AND), or this value is set to True when any of the Output n Priority inputs are not 0 or 16 (OR).

OR

Set Name: AND/OR

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)