Reliability (Heat Recovery Suitability Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Heat Recovery Suitability output is set to None if the OA Temperature, Exhaust Air Temperature, or the Low Limit Process Variable inputs are not reliable.