Module Use in Application (Waterside Economizer Sequencer) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the name in the following table.

Table 1. Waterside Economizer Sequencer Uses in Application System Selection Trees

Module Instance Name

Application

Waterside Economizer Sequencer

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.