Tower Start Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Tower Start Determination module enables the cooling tower subsystem whenever the system enable is true, or a condenser water pump is on. This module monitors the System Enable input and the CW Pump Sequencer. The cooling tower subsystem is not disabled until System Enabled is False, all condenser water pumps are off, and a user-defined delay has expired. This module has inputs for the user-defined delay, System Enabled, and the number of active pumps. It has a single state output which indicates whether the cooling tower subsystem should be enabled or disabled.

Figure 1. Tower Start Determination