The System Enable module enables or locks out a heating or cooling device. This module accepts as inputs outdoor air temperature, outdoor air enable setpoint, outdoor air enable differential, heating/cooling selection, and a network isAvailable. The module has a state output that indicates if the module is enabled.
You can view and modify the modules in this group’s logic.