Module Use in Applications (Secondary Bypass Valve Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the module names in the following table.

Table 1. Secondary Bypass Valve Sequencing Uses in Application System Selection Trees
Module Instance Name Applications
Secondary Bypass Valve Sequencing

Central Cooling Applications

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.