Module Use in Applications (Plant Sequencing-OA-T) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Plant Sequencing-OA-T Uses in Application System Selection Trees

Module Instance Name

Applications

Boiler Sequencing by OA-T

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.