Primary States (Plant Sequencing-Decouple) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
  • Off: Indicates the system is disabled.

  • Pump Only: Allows a circulation pump to run as a minimum whenever the system is enabled.

  • System Interlock: Allows a global system interlock to be turned on prior to starting any stages.

  • Control: Allows the output value to change to meet the demand of the system.