The following table describes the attributes used by the Load Calculation modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Flow |
Indicates the rate the media is moving through the system. |
0 Display Units: l/s, gpm |
|
Glycol Concentration |
Indicates the percentage of Glycol in the system. |
0 Display Units: % |
|
HeatingCooling |
Switches the Load output, so a positive value is output for either a Heating or Cooling Mode. |
Heating Set Name: Heating/Cooling |
|
Load |
V |
Indicates the calculated Load. |
0 Display Units: W, Btuh |
Media |
Indicates the type of media used in the system. |
Water Set Name: Load Media |
|
Return Temperature |
Indicates the temperature of the media returning from the system. |
0 Display Units: °C, °F |
|
Supply Temperature |
Indicates the temperature of the media supplied to the system. |
0 Display Units: °C, °F |
|
Unit Set |
Switches the calculation based on the application’s system of units. |
IP Display Units: SI, IP |