Module Use in Applications (Device Enable Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Device Enable Determination Uses in Application System Selection Trees

Module Instance Name

Application

Chiller Enable Determination

Central Cooling with Optimization Applications

Cooling Tower Enable Determination

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.