Module Use in Applications (Device Availability Calculation, Count True Inputs) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Device Availability Calculation Uses in Application System Selection Trees

Module Instance Name 1

Applications

Boilers Available

Central Heating Applications

CWPs Available

Central Cooling Applications

CW Pump Capacity Check

Central Cooling with Optimization Applications

PCHWPs Available

Central Cooling Applications

Towers Available

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.

1 The Count True Inputs palette item appears in the Setpoint Determination/Misc column, but the module instances appear in the State Generator and Output Controller columns of the UI.