Device Availability Calculation (Count True Inputs) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Device Availability Calculation module calculates the number of available devices that are able to run. This module accepts eight device enable inputs as well as a limit input value that acts as a high limit. Based on the input commands and the attribute settings, the module outputs a number (floating value) of devices that are currently available.

You can view and modify the modules in this group’s logic.